Other Parts Discussed in Thread: ADS1211
We are using an anolog to digital converter called as ADS1211 in our project. However, a serious problem has been occured about this IC. Digital data ,which is read from ADS1211, changes with apporoximately one hundred seconds period and ten seconds duty cycle. Figure of it is attached below. We use two different system design for converting process but same problem was occured at both of them. Configuration settings that we used are like that:
Turbo mode: 1
Gain: 1
Data rate: 1000Hz,673Hz,100Hz
Reference: Internal , External
XClk: 10 MHz, 2MHz
Bias: Off
Data Format: Offset Binary
U/B : Unipolar
Operating Mode: Normal Mode
Could you give a feedback about this problem as soon as possible, please.
Best Regards
Mehdi Duman
R&D Engineer TUBITAK SAGE