This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC60704: AMC60704

Part Number: AMC60704


Tool/software:

Screenshot as above, issues encountered in debug:

1. VCC_MCU=3.3VDC, VCC_5V=5VDC, VCC_LASER=1.55VDC, are there any power supply sequence and timing requirements for these power supplies?

2. When IDAC/VDAC/ADC is not normally external load or input in PCBA debug, VDAC cannot test the normal set voltage. The current  VDAC measured voltage is 0VDC, and I2C cannot read the normal value after the ADC get voltage.

Emergency help, thanks