Part Number: DAC3482
Other Parts Discussed in Thread: CDCE62005
Tool/software:
I am evaluating the DAC3482 for a new product design. Currently I am using the DAC3482-EVM board, and the FMC adaptor board. I am driving the SPI using the supplied TI software DAC38x GUI.
I am generating a ramp using an in-house FPGA board. The ramp has been verified on an oscilloscope. I use the CDCE62005 secondary reference (on board crystal) to generate all the clocks including the FPGA input clock. This in turn generates the data clock and FIFO strobe signals.
What I would expect to see is my ramp on the output of the DAC. Instead, I see _nothing_ However, when I enable the mixer (which I would think I could bypass) I now see my ramp, but with an oscillation inside the envelope. Nothing I do seems to affect the frequency of the oscillation. Please help explain the following:
How do I configure the DAC to just output the DC signals sent in on the parallel bus (no mixer, no NCO, etc)?
What is causing the output I see?
Why do I need the mixer enabled?
We want to use this as a straight-forward DAC at 250MSPS. I do not see another alternative, but if you can suggest a better product, I am open to changing the design.
Thanks
Ben
Attachments: Traces
`default_nettype none
`timescale 1ns / 1ps
//////////////////////////////////////////////////////////////////////////////////
// Company: RedWave Labs Ltd
// Engineer: BCK
//
// Create Date: 07.11.2022 12:17:14
// Design Name: DAC3482
// Module Name: top
// Project Name:
// Target Devices:
// Tool Versions:
// Description: Drives ramp into DAC
//
// Dependencies:
//
// Revision:1.0
// Revision 0.01 - File Created
// Additional Comments:
//
//////////////////////////////////////////////////////////////////////////////////
module top(
output wire rx_serial,
input wire tx_serial,
output wire led_pl_green,
output wire led_pl_red,
output wire o_SYNTH_CTRL_CE,
output wire[0:2] tp,
output wire[15:0] D_P,
output wire[15:0] D_N,
output wire FIFO_ISTR_N,
output wire FIFO_ISTR_P,
input wire EVAL_FPGA_CLK_N,
input wire EVAL_FPGA_CLK_P,
output wire DATA_CLK_N,
output wire DATA_CLK_P,
output wire SYNC_N,
output wire SYNC_P
);
// use the startup block clock for the UART
wire sys_clk;
reg ce_off = 1'b0;
assign o_SYNTH_CTRL_CE = ce_off;
STARTUPE2 STARTUPE2
(
.CLK(1'b0),
.GSR(1'b0),
.GTS(1'b0),
.KEYCLEARB(1'b1),
.PACK(1'b0),
.PREQ(),
.USRCCLKO(1'b0),
.USRCCLKTS(1'b0),
.USRDONEO(1'b0),
.USRDONETS(1'b1),
.CFGCLK(),
.CFGMCLK(sys_clk),
.EOS()
);
wire dac_data_clk;
reg [15:0] dac_data = 16'b0;
// module to convert single-ended data to LVDS:
dac_driver dac1 (
.data_in(dac_data),
.data_out_p(D_P),
.data_out_n(D_N),
.clk_in(dac_data_clk),
.frame_n(FIFO_ISTR_N),
.frame_p(FIFO_ISTR_P),
.sync_n(SYNC_N),
.sync_p(SYNC_P)
);
wire dac_data_clk_int;
// EVAL board generates a clock for us. Use as data clock
IBUFDS IBUFDS_dac_clk (
.O(dac_data_clk_int),
.IB(EVAL_FPGA_CLK_N),
.I(EVAL_FPGA_CLK_P)
);
OBUFDS #(
.IOSTANDARD("LVDS"), // Specify the output I/O standard
.SLEW("FAST") // Specify the output slew rate
) OBUFDS_dac_clk (
.I(dac_data_clk_int), // Diff_p output (connect directly to top-level port)
.OB(DATA_CLK_N), // Diff_n output (connect directly to top-level port)
.O(DATA_CLK_P)
);
BUFG BUFG_clk (.I(dac_data_clk_int), .O(dac_data_clk));
// UART decoder
(* mark_debug = "true" *) wire [7:0] ser_data;
(* mark_debug = "true" *) wire dv;
wire uart_clk;
clock_divider #(.DIVISOR(10)) cd0 (sys_clk, uart_clk);//65kHz
assign rx_serial = tx_serial; //echo back serial command
//564 at 65MHz is baud 115200
//6771 at 65MHz is baud 9600
uart_rx #( .CLKS_PER_BIT(677)) uart1
(
.i_Clock(uart_clk),
.i_Rx_Serial(tx_serial),// inverted: names wrt PC!
.o_Rx_DV(dv),
.o_Rx_Byte(ser_data)
);
// three modes. Constant value, triangle or sine
reg triangle_en = 1'b0;
reg [15:0] const_dac = 16'b0;
reg sine_en = 1'b0;
// command decoder
always @ (posedge(sys_clk))
begin
case(ser_data)
"T": //start triangle output
triangle_en <= 1'b1;
"t": //stop triangle output
triangle_en <= 1'b0;
"0": //set constant to minimum (signed int)
const_dac <= 16'hFFFF/2;
"3": //set constant to 0.25 max (signed int)
const_dac <= 16'h7FFF/4;
"5": //set constant to 0.5 max (signed int)
const_dac <= 16'h7FFF/2;
"7"://set constant to 0.75 max (signed int)
const_dac <= 16'h7FFF/4*3;
"9": //set constant to max (signed int)
const_dac <= 16'h7FFF;
"S": //start sine wave output
sine_en <= 1'b1;
"s"://stop sine wave output
sine_en <= 1'b0;
endcase
end
wire [7:0] sine;
reg [15:0] dac_value = 16'b0;
//reg [15:0] bit =16'b0;
reg dir = 1'b0;
always @ (posedge(dac_data_clk))
begin
if(triangle_en) begin
if(dir == 0)
dac_value <= dac_value +1;
if(dir == 1)
dac_value <= dac_value -1;
end else begin
dac_value <= const_dac;
end
if(dac_value == 16'h7FFE )
dir <= 1'b1;
if(dac_value == 16'h1 )
dir <= 1'b0;
// walking bit used for digital testing:
//bit <= 1<< dac_value[5:0];
end
//convert triangle to sine using lookup:
sine_table st1 (.i_clk(dac_data_clk), .i_ce(sine_en), .i_phase(dac_value[7:0]), .o_val(sine));
always @(*) begin
if(sine_en)
dac_data <= {1'b0, sine, 7'b0}; // largest value for signed int
else
dac_data <= dac_value;
end
//various debug on LED and test-pins
wire dac_data_clk_div_1000;
clock_divider #(.DIVISOR(1000)) cd1 (dac_data_clk, dac_data_clk_div_1000);//300kHz
wire led_flash;
clock_divider #(.DIVISOR(32500000)) cd2 (sys_clk, led_flash);//2Hz
assign tp[0] = dac_data_clk_div_1000;
assign tp[1] = dv;
assign tp[2] = triangle_en;
assign led_pl_green = led_flash;
assign led_pl_red = triangle_en;
endmodule
`default_nettype wire
x00 x0198 x01 x106E x02 x8052 x03 xF000 x04 xFFFF x05 x3E60 x06 x2800 x07 xFFFF x08 x0000 x09 x8000 x0A x0000 x0B x0000 x0C x0400 x0D x2400 x0E x0400 x0F x0400 x10 x3000 x11 x0000 x12 x0000 x13 x0000 x14 x1388 x15 x0000 x16 x3333 x17 x3333 x18 x4C78 x19 x2804 x1A x1410 x1B x0800 x1C x0000 x1D x0000 x1E x1111 x1F x1110 x20 x4401 x22 x1B1F x23 x00FF x24 x0000 x25 x7A7A x26 xB6B6 x27 xEAEA x28 x4545 x29 x1A1A x2A x1616 x2B xAAAA x2C xC6C6 x2D x0001 x2E x0000 x2F x0000 x30 x7530 x7F x0004 CDCE62005 Registers Freq:0.000000MHz Address Data 00 01400100 01 811C0101 02 81400102 03 C1400103 04 01040104 05 29F01B65 06 44AE0016 07 165294A7 08 20001808