Part Number: DAC8775
Tool/software:
Hi,
We use the DAC8775 in our PLC AO-module project.
Now we test the Settling Time of DAC8775 but the waveform is about more than 1ms, it is slow that it is only 15-30us in the datasheet, please kindly review our schematic diagram,
provide your comment if there are any error;
Our design: output 4channels, and 0-10V range.
the below waveform is the the rise time is 1ms, the fall time is 6ms, the SW configuration is default: