Part Number: ADS131M08EVM
Tool/software:
Hi~
1KHz square wave was applied to ads131m08evm.
If the sampling rate is set to 4k in the ads131m08evm program, it is measured as a triangle wave instead of a square wave.
At 32k sampling rate a square wave shape appears, but it is not the same square wave waveform as the source.
Attached is the 1KHZ SORCE waveform, EK sampling 1K/4K/16K/32K measurement waveform.
Nyquist Theorem says that the sampling rate should be more than twice.
1. When the sampling rate is 4k, why is it measured as a triangle wave and how to obtain the same signal as the original signal?
2. Why is it different from the original signal even when it is 32K?
3. What is the sampling rate to restore the same as the original signal?
Thanks~