Part Number: ADS124S08
Tool/software:
Hello,
Designed a circuit to Measure Temperature using RTD.The SPI interfaces are working fine, but the Exitation current is Zero, though its SET to 1uA.Schematics attached.
The Analog voltage and Digital voltage is 3.3.V,
Exitation current is 1mA,
PT 1000 RTD is used..

The AIN0 is configure as a current source pin.
Is there there anything else to consider to enable the current flow. ? is the head room of 0.7v oke in the current source path ?
Thanks,
Sobin