Tool/software:
When we developed AFE5818, under the same input signal and the same configuration conditions, we found that the AFE5818 circuit board developed by ourselves was nearly 10 times less than the official development board signal provided by AFE5818. Could you please help us see the reason
When the input signal is 5Mhz 50mV and the upper computer software is configured as the maximum gain, the actual signal acquisition situation is as shown in the figure below
1) The data acquisition waveform of AFE5818EVM official development board is limited
2)AFE5818 self-developed circuit board data acquisition waveform