This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: ADS1263 - Frequency response in FIR configuration ?

Part Number: ADS1263


Tool/software:

Hi,

In the ADS1263 datasheet it is stated that using the FIR digital filter we have the combination of:

- First stage filter, 'sinc5' shape, with output rate of 14 400 SPS (fig 9.15) using internal oscillator

- Second stage filter with output rate of 600 Hz

- Then FIR stage with output rate of 20 SPS and shape is in Fig 9.22

The problem is that we don't know the filter response of the second stage is this configuration : we know it decimates from 14 400 down to 600 SPS but with what frequency shape ?

Is figure 9.22 a combination of FIR stage + second stage or only the FIR stage ?

Has the second stage a 'sinc1' filter shape ?

What is the overall filter shape from input to the FIR output at 20 Hz ?

Thank you.

  • Hi Damien Buisson,

    The sinc filter transfer function is given by equation 14, so that should be very clear for every filter type other than the FIR

    We do not provide an equation for the FIR filter, but we provide frequency plots in section 9.3.10.2. These plots represent the complete frequency response of all filter stages

    -Bryan