Part Number: ADS1178
Tool/software:
Hi,
I have used "ADS1178IPAPR" part in one of my design to read the analog data. Below is the connection. Below are some of the configuration set on the board. But I am having trouble in getting the DRDY signal. Any suggestions?
Configurations:
Format [2:0] - 000
Mode : 0
Test 0:1 : 00
CLKDIV - 3.3V
IOVDD-3.3V
DVDD - 1.8V
AVDD- 5V
Clk - 27MHz