Other Parts Discussed in Thread: TX7332
Tool/software:
Hi,
We are currently using the AFE5832 chip in the design of a handheld ultrasound device. While developing the driver for the AFE5832, we encountered an issue that we hope you can help us resolve.
In test pattern mode (Ramp), our driver functions correctly, as demonstrated in the first attached figure. However, when we switch to normal operating mode, the driver fails to properly receive the input signal, as shown in the second attached figure. We initially considered whether the input signal might be out of range, but our differential input is INP: 1.6V and INM: 1.2V, with no additional input voltage.
In normal operating mode (TGC mode), in addition to the chip configurations used in test pattern mode, we have set the following:
- TGC mode
- LNA_GAIN set to 15dB
- PGA_GAIN set to 21dB
- Programmable Attenuator gain code set to default (0)
- Input channel INP set to 1.6V
- Input channel INM set to 1.2V
Despite these configurations, we are unable to achieve normal operation. Are there any additional chip configurations or settings that we need to adjust to resolve this issue? Your guidance and support in this matter would be greatly appreciated.