Other Parts Discussed in Thread: ADS1230
Dear Bob,
Thank you for your quick reply...Actually in my project interfacing pic16f877a interfacing ADS1230,I m using 6Kg load cell.So i can easily achieve the accuracy of 1gram.But if i m using the larger capacity load cell (example:50kg,100kg capacity) its difficult to get 1 gram accuracy,so its better to use 5 gram accuracy(i.e. each division shows 5 gram ).So the reading shows like 00000,00005,00010,00015....etc.
But my reading looks like 00000,00001,00002,00003......etc(i.e. 1 gram division).
So my doubt is how to make 5 gram division, if i m using 50kg load cell.That is i need the readings like 00000,00005,00010,00015,00020....etc.
So what change should i make in my formula...Please Help....Thanks IN ADVANCE..
By
Ajith.