Part Number: ADS131M08EVM
Tool/software:
Team,
Can you please help answer these questions:
My customer would like to use the main ADC board without the PHI board, therefore they just need to make sure the SPI interface can be driven from the pin header. The documentation seems to suggest that it can. Can you confirm?
Also, if they are not using the PHI board what would they have to provide to the ADC main board?
- Power?
- Clock?, etc.
- The voltage input can be scaled by changing the voltage divider resistors on the board, right?
Thanks
Viktorija