Part Number: ADS7044
Other Parts Discussed in Thread: ADS7054
Tool/software:
Hello support,
I am working on two projects using ADS70xx family.
- project 1: using ADS7044 (12 bits)
- project 2: using ADS7054 (14 bits)
I would like to clarify what is the data output when performing a single cycle, because this is explained differaly between the two datasheet:
ADS7044:

ADS7054:

Can you confirm whether the data output during cycle N for ads7044 is the data from sample N, and whether the data output during cycle A for ads7054 is the data from the previous sample (A-1) ? If this is the case, it means that both device works differently:
for the ads7044, the latest data can be obtained by running only one cycle.
for the ads7054, the latest data can be obtained by running two cycles: the first for acquisition and the second for sending the data.
thank you,