Part Number: ADC12D800RF
Tool/software:
I have been using this ADC12D800RFRB board for a few months i am working on partial discharge detection and measurements in high power apparatus using ultra high frequency (UHF) sensor. The UHF sensors are broadband antennas operating from 0.5 to 3 GHz frequency range and the PD signal's spectral content in UHF regime spans over 0.4 to 2 GHz. PD emissions are stochastic by nature and the emissions give out several bursts lasting for about 1 ns. I was unable to capture this signal with this ADC12D800RFRB i tried sending a continuous stream of pulses through a arbitrary waveform generator i could see the continuous signals being captured in wave vision 5 software but i was not able to see or capture burst signal i hope the buffer is full or can i program the board so that it would be useful for my application can anyone help me out