Tool/software:
Dear all,
I am validating a design that uses 4 ADS1298 in cascaded configuration. For all of the ADS1298, I can read their ID, read/write to config register 1,2,3 and config individual channels.
However, when I put the devices in continuous data reading mode at 2KHz, there is nothing coming from the ADCs, not even the status word, though the data ready pin was toggling correctly at 2KHz.
As documented in Section 9.4.1.3.1, the status word should have 1100 in the leading bits. But all the data from the ADC are 0s.
You can find my probed result (with Saleae Logic 1 software) in the attached.
I appreciate any insight from you. Thank you very much.
Best,
Aiden