Tool/software:
Hi,
I am using ADS1298ECG-FE Board And applying +/-500mV sine wave at 100Hz frequency at input as shown below in figure-1.

Figure-1 : Input of ADS1298
We are able to achieve complete sine wave in EVK as applied to input. Output of EVK kit is shown in figure-2.
Figure-2 : Output of EVK Kit from Software
But when we use ADS1298 Board with the Nordic NRF52840-DK Noise is Affecting our signal. We are collecting data through SPI and sending data to USB through NRF, After that we are plotting the graph and the noise is visible in the graph as shown in figure-3 provided below.
Figure-3 : Output Of USB captured through NRF
I Found that there is on Board DSP in EVK kit, So is there any kind of mechanism provided in DSP software to filter out noise? If yes, what is it?
We have done complete jumper setting as mentioned in datasheet as well as Ti Fourm. Below is the register configurations we have done.
conf|config1 0x01 0x81 conf|config2 0x02 0x10 conf|config3 0x03 0xDC conf|loff 0x04 0x03 conf|ch1set 0x05 0x20 conf|ch2set 0x06 0xA0 conf|ch3set 0x07 0xA0 conf|ch4set 0x08 0xA0 conf|ch5set 0x09 0xA0 conf|ch6set 0x0A 0xA0 conf|ch7set 0x0B 0xA0 conf|ch8set 0x0C 0xA0 conf|rldsensp 0x0D 0xFF conf|rldsensn 0x0E 0xFF conf|loffsensp 0x0F 0xFF conf|loffsensn 0x10 0x02 conf|loffflip 0x11 0x00 conf|gpio 0x14 0x00 conf|pace 0x15 0x00 conf|resp 0x16 0xF0 conf|config4 0x17 0x22 conf|wct1 0x18 0x0A conf|wct2 0x19 0xE3