I have been reviewing the ADS1258 datasheet and I notice that it can be configured to use several set data sampling rates. From what I understand, the lower the sampling rate, the more digital filtering is done on the signal data. We may need to sample at a variety of rates, some lower than those listed as a configurable option. What would the be the best way to sample the ADC lower than the configured rate and what implications would there be in doing so?
Thanks!