Part Number: ADS127L01
Tool/software:
I am using the ADS127L01 in frame sync master mode, where each reading from the ADC has a 4-bit CRC using the CRC-4-ITU algorithm. Does anyone have a table driven (or similarly efficient) software implementation of calculating this CRC? I have a "simple" bit by bit implementation, but it is quite slow.
I am using the ADS127L01 in frame sync slave mode, and I have questions. crcany provides a table driven implementation, but I haven't got it working yet. My questions:
- The datasheet says "Begin with the MSB in the data stream." I've got 32 bits: 24 bits of data and an 8-bit status word. So, if I call the status word byte 0, I want to perform the CRC over bytes 3, 2, and 1. The table driven CRC calculator works on a byte at a time. The MSB would be in byte 3, right? So, I need to feed the CRC calculator bytes 3, 2, and 1, in that order?
- Is the CRC over a single frame (24 bits in this configuration)? The datasheet says "Set the shift register to all zeros." Do I reset the CRC shift register for each frame, or should it be preserved for the next frame?
- Greg Cook's catalog gives the parameters for CRC-4/ITU as width=4 poly=0x3 init=0x0 refin=true refout=true xorout=0x0 check=0x7 residue=0x0 name="CRC-4/G-704" (see Model parameters). "width", "poly", and "init" are in accord with the datasheet. refin=true, however, says the characters are read bit-by-bit, least significant bit (LSB) first, which seems contrary to the datasheet. refout=true specifies that the results are reflected, character-by-character, but in this case we don't even have a whole character. I don't know which parameters to use to match the ADS127L01.
This is the crcany code I'm trying to use:
static unsigned char const table_byte[256] = {
0x90, 0xa0, 0xf0, 0xc0, 0x50, 0x60, 0x30, 0x00, 0x20, 0x10, 0x40, 0x70, 0xe0,
0xd0, 0x80, 0xb0, 0xc0, 0xf0, 0xa0, 0x90, 0x00, 0x30, 0x60, 0x50, 0x70, 0x40,
0x10, 0x20, 0xb0, 0x80, 0xd0, 0xe0, 0x30, 0x00, 0x50, 0x60, 0xf0, 0xc0, 0x90,
0xa0, 0x80, 0xb0, 0xe0, 0xd0, 0x40, 0x70, 0x20, 0x10, 0x60, 0x50, 0x00, 0x30,
0xa0, 0x90, 0xc0, 0xf0, 0xd0, 0xe0, 0xb0, 0x80, 0x10, 0x20, 0x70, 0x40, 0xe0,
0xd0, 0x80, 0xb0, 0x20, 0x10, 0x40, 0x70, 0x50, 0x60, 0x30, 0x00, 0x90, 0xa0,
0xf0, 0xc0, 0xb0, 0x80, 0xd0, 0xe0, 0x70, 0x40, 0x10, 0x20, 0x00, 0x30, 0x60,
0x50, 0xc0, 0xf0, 0xa0, 0x90, 0x40, 0x70, 0x20, 0x10, 0x80, 0xb0, 0xe0, 0xd0,
0xf0, 0xc0, 0x90, 0xa0, 0x30, 0x00, 0x50, 0x60, 0x10, 0x20, 0x70, 0x40, 0xd0,
0xe0, 0xb0, 0x80, 0xa0, 0x90, 0xc0, 0xf0, 0x60, 0x50, 0x00, 0x30, 0x70, 0x40,
0x10, 0x20, 0xb0, 0x80, 0xd0, 0xe0, 0xc0, 0xf0, 0xa0, 0x90, 0x00, 0x30, 0x60,
0x50, 0x20, 0x10, 0x40, 0x70, 0xe0, 0xd0, 0x80, 0xb0, 0x90, 0xa0, 0xf0, 0xc0,
0x50, 0x60, 0x30, 0x00, 0xd0, 0xe0, 0xb0, 0x80, 0x10, 0x20, 0x70, 0x40, 0x60,
0x50, 0x00, 0x30, 0xa0, 0x90, 0xc0, 0xf0, 0x80, 0xb0, 0xe0, 0xd0, 0x40, 0x70,
0x20, 0x10, 0x30, 0x00, 0x50, 0x60, 0xf0, 0xc0, 0x90, 0xa0, 0x00, 0x30, 0x60,
0x50, 0xc0, 0xf0, 0xa0, 0x90, 0xb0, 0x80, 0xd0, 0xe0, 0x70, 0x40, 0x10, 0x20,
0x50, 0x60, 0x30, 0x00, 0x90, 0xa0, 0xf0, 0xc0, 0xe0, 0xd0, 0x80, 0xb0, 0x20,
0x10, 0x40, 0x70, 0xa0, 0x90, 0xc0, 0xf0, 0x60, 0x50, 0x00, 0x30, 0x10, 0x20,
0x70, 0x40, 0xd0, 0xe0, 0xb0, 0x80, 0xf0, 0xc0, 0x90, 0xa0, 0x30, 0x00, 0x50,
0x60, 0x40, 0x70, 0x20, 0x10, 0x80, 0xb0, 0xe0, 0xd0};
// https://github.com/madler/crcany
unsigned crc4interlaken_byte(unsigned crc, void const *mem, size_t len) {
unsigned char const *data = mem;
if (data == NULL)
return 0;
crc &= 0xf;
crc <<= 4;
while (len--)
crc = table_byte[crc ^ *data++];
crc >>= 4;
return crc;
}
I also tried:
static unsigned char const table_byte[256] = {
0x0, 0x7, 0xe, 0x9, 0x5, 0x2, 0xb, 0xc, 0xa, 0xd, 0x4, 0x3, 0xf, 0x8, 0x1, 0x6,
0xd, 0xa, 0x3, 0x4, 0x8, 0xf, 0x6, 0x1, 0x7, 0x0, 0x9, 0xe, 0x2, 0x5, 0xc, 0xb,
0x3, 0x4, 0xd, 0xa, 0x6, 0x1, 0x8, 0xf, 0x9, 0xe, 0x7, 0x0, 0xc, 0xb, 0x2, 0x5,
0xe, 0x9, 0x0, 0x7, 0xb, 0xc, 0x5, 0x2, 0x4, 0x3, 0xa, 0xd, 0x1, 0x6, 0xf, 0x8,
0x6, 0x1, 0x8, 0xf, 0x3, 0x4, 0xd, 0xa, 0xc, 0xb, 0x2, 0x5, 0x9, 0xe, 0x7, 0x0,
0xb, 0xc, 0x5, 0x2, 0xe, 0x9, 0x0, 0x7, 0x1, 0x6, 0xf, 0x8, 0x4, 0x3, 0xa, 0xd,
0x5, 0x2, 0xb, 0xc, 0x0, 0x7, 0xe, 0x9, 0xf, 0x8, 0x1, 0x6, 0xa, 0xd, 0x4, 0x3,
0x8, 0xf, 0x6, 0x1, 0xd, 0xa, 0x3, 0x4, 0x2, 0x5, 0xc, 0xb, 0x7, 0x0, 0x9, 0xe,
0xc, 0xb, 0x2, 0x5, 0x9, 0xe, 0x7, 0x0, 0x6, 0x1, 0x8, 0xf, 0x3, 0x4, 0xd, 0xa,
0x1, 0x6, 0xf, 0x8, 0x4, 0x3, 0xa, 0xd, 0xb, 0xc, 0x5, 0x2, 0xe, 0x9, 0x0, 0x7,
0xf, 0x8, 0x1, 0x6, 0xa, 0xd, 0x4, 0x3, 0x5, 0x2, 0xb, 0xc, 0x0, 0x7, 0xe, 0x9,
0x2, 0x5, 0xc, 0xb, 0x7, 0x0, 0x9, 0xe, 0x8, 0xf, 0x6, 0x1, 0xd, 0xa, 0x3, 0x4,
0xa, 0xd, 0x4, 0x3, 0xf, 0x8, 0x1, 0x6, 0x0, 0x7, 0xe, 0x9, 0x5, 0x2, 0xb, 0xc,
0x7, 0x0, 0x9, 0xe, 0x2, 0x5, 0xc, 0xb, 0xd, 0xa, 0x3, 0x4, 0x8, 0xf, 0x6, 0x1,
0x9, 0xe, 0x7, 0x0, 0xc, 0xb, 0x2, 0x5, 0x3, 0x4, 0xd, 0xa, 0x6, 0x1, 0x8, 0xf,
0x4, 0x3, 0xa, 0xd, 0x1, 0x6, 0xf, 0x8, 0xe, 0x9, 0x0, 0x7, 0xb, 0xc, 0x5, 0x2};
unsigned crc4g_704_byte(unsigned crc, void const *mem, size_t len) {
unsigned char const *data = mem;
if (data == NULL)
return 0;
crc &= 0xf;
while (len--)
crc = table_byte[crc ^ *data++];
return crc;
}
The difference is in reflection.