Other Parts Discussed in Thread: ADS1299,
Tool/software:
Hi,
I bought the ADS1299EEGFE-PDK, but I don't want to use the accompanying MMB0. I want to use the STM32 to control the ADS1299, but I have some questions:
1. Do I only need to use a jumper to connect the power terminal in the J5 connector on the MMBO to J4 on the ADS1299EEGFE-PDK to power the ADS1299EEGFE-PDK? Then use the required pins on J3 of the ADS1299EEGFE-PDK to connect with the STM32?
2. If I want to use the STM32 to read the register value in the ADS1299, do I only need to connect CS, MOSI, MISO, SCLK in J3 with the STM32?
Regards,
Junzhe