Part Number: ADC3662
Tool/software:
Hi,
is there always a hardware reset needed after power-up phase?
If yes, would it also be possible to keep the RESET pin at high from beginning, so:

Thanks for help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC3662
Tool/software:
Hi,
is there always a hardware reset needed after power-up phase?
If yes, would it also be possible to keep the RESET pin at high from beginning, so:

Thanks for help!
Hi Simon,
A hardware reset is advised such that the registers reset to a known state each and every time the device is powered on. It is an active high signal that should be toggled only after the supplies have all settled. If you leave it high while the supplies are turning on, we cannot guarantee the register state across power cycles.
The normal practice is to use a watchdog circuit based on the last power rail to come up, in this case, AVDD18. The diagram shows to assert reset after REFBUF is stable, but since the REFBUF can be used for bootstrap selection, it's better to place the watchdog on the AVDD rail and the watchdog delay will account for the time that REFBUF settles. This circuit below will work for the active high reset this part requires.

Thanks, Chase
Hi Simon,
The hardware reset is so the registers reset to a known state each and every time the device is powered on. If you trigger software reset this will also accomplish the same, however many customers require a known device state immediately at power up, which is why our devices have a hardware reset.
Thanks, Chase