This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M08EVM: GUI secondary Y-scale is not correct

Part Number: ADS131M08EVM


Tool/software:

I'm using the ADS131M08EVM and software, I configured a channel to use DC test voltage signal.

When I take the capture, the GUI voltage scale is not updated correctly, its showing 0.154V to 0V total range.

I noticed the measurement (and codes) are tighter and more closer to expected ~0.16V from the test signal and I can get closer to this value with gain calibration.

Once I toggle the Y scale fit parameter the secondary axis corrects itself.

Just an issue with software, maybe need to update the loop to rescale that secondary Y scale. 

Hope this helps,

-Orlando