This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8812: SW lib for DAC8812

Part Number: DAC8812
Other Parts Discussed in Thread: DAC8811,

Tool/software:

Team,
Do we have a SW lib or some SW example example that can be used for DAC8811/DAC8812?

Thank in advance!

Anthony

  • Hi Anthony, 

    No, we typically don't provide software examples as every type of controller is different. You can likely find SPI software examples for the controller you are using and adapt them to work with our device. The SPI interface for the DAC8812 is very simple. There is an 18-bit data frame that consists of 2 address decode bits, and the 16-bit DAC data:

    Best,

    Katlynne Jones