Other Parts Discussed in Thread: ADS131M08
Tool/software:
Using the ADS131M08EVM software, and things are good in the high resolution mode.
I am able to hook up a function generator, and measure the 100Hz sine wave I'm generating, and see the FFT.
When I change to low-resolution mode, the sample rate goes down 1/2 which was fine initially.
However the time domain wave is unexpectedly the same when it should be elongated, so it appears the sample rate in hardware is actually not changed.
The frequency domain's fundamental frequency is divided by 1/2, reporting a 50Hz wave, despite no change to the FGEN 100Hz output.
Essentially, low power mode is giving me half of the expected frequency, and I believe there's some software issue with this.
I also suspect very-low power mode divides the frequency by another 1/2, ie going to report to me a 25Hz wave when the FGEN is generating 100Hz.