Other Parts Discussed in Thread: ADS122C04, TLA2528, ADC081C021, ADS1119
Tool/software:
Hi,
Is there an I2C based ADC that can support around 20 or more I2C addresses?
I'm trying to implement a self test feature on a board using TMP1075DSGR for temperature and some ADC.
TMP1075DSGR can support 32 addresses which makes it possible for me to use point of load topology.
However every ADC I've looked at is capped at 9 addresses. Most of them at 4.
Ideally I would be able to find a 1 channel ADC that is in a small package, and can support 32 addressers to match the temperature sensor.
But I could also make a4 channel ADC work if it can support at least 16 addresses and is still a small package.
It's just for measuring voltage supplies.
Speed is not a factor.
Resolution is also barely a factor since I only care if my voltages are within a 5% tolerance, measured through dividers.