Other Parts Discussed in Thread: OPA328
Tool/software:
Hello,
how large is the reference capacitor CREF on the ADS127L11?

I need the value to simulate if my external reference voltage buffer settles fast enough.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello FZ,
The equivalent reference input capacitance for ADS127L11 is 10pF. Note that is you use the REFP buffer, the equivalent input capacitance is reduced by more than 100x.
Regards,
Keith Nicholas
Precision ADC Applications
Hello Keith Nicholas,
thank you very much.
The internal REFP buffers must be deactivated because I want to operate the ADC with AVDD1=3.3V (low-speed mode) and use a 3.0V reference.
I am planning to use the OPA328 (as shown in sboa558) to buffer the REF35300 voltage reference.
On my simulations, the reference voltage settles fast enough (using fmod=1.6385MHz).
Do you think this buffering circuit is suitable for this application?
Hello FZ,
Yes, the OPA328 will have more than enough bandwidth to drive the ADS127L11 REFP input.
Regards,
Keith