Part Number: ADS131E08
Other Parts Discussed in Thread: ADS131M08,
Tool/software:
Hi all,
I am developing a modular data acquisition system for cryogenic temperature devices. This system currently is based around the ADS131m08 ADCs which appear to be a very cost effective way to achieve the performance I need. However, the E family of chips offers a few features that I would benefit from greatly - 2.5V reference support and high input impedance at unity gain.
I am considering switching a subset of the ADCs to the E family however as the system is modular I would require both of these to work "together". Working together just means sharing a clock and being synchronized.
I see that the E08 has a much stricter clock requirement (2Mhz) which the M08 chip will accept. The M08 chip is synchronized by pulsing the SYNC/RESET pin low for a few clock periods while the E08 has a START pin which the datasheet indicates can be used by multiple ADCs to sync them.
My question is as follows: can I tie the START pin of a ADS131E08 to the SYNC/RESET pin of the ADS131M08 and sync all devices by generating a short low pulse to sync all devices? The low state will sync the M08 devices and my understanding of the E08 datasheet implies that the rising edge will sync the E08 devices. The timing requirements of the E08 do not explicitly state the minimum pulse duration for a START condition to occur.
Thank you all for your advice!
Bonus question: The M08 has ESD protection which means that with a large enough series resistor the inputs of the device are not damaged if my input circuitry rails for some reason, does the E08 have these as well?