This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC08DJ5200RFEVM: How to set the sampling frequency without using ADCxxDJxx00RF EVM GUI?

Part Number: ADC08DJ5200RFEVM


Tool/software:

I can set the clock and parameters on the board via this GUI from TI. But I want to know if I can write to the register of the clock chip and the adc chip without using this GUI since it's possible that I may need to send the command from linux. It's also possible I will use the SPI port from FMC+. I have seen the jumper to control the spi source as below.