Other Parts Discussed in Thread: DAC39RF10EVM, DAC39RF10
Tool/software:
Hi,
There is issue 3dB lower output power than expectation.
Please check below questions.
1. Can it increase output power level with increasing switched output current by modifying Rbias?
2. Customer tried to input -3.6V instead of -1.8V at VEEAM18 and VEEBM10. can it make this lower output? now it's connected to -1.8V.
Thanks.