This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7138: Driver support for LINUX Kernel 5.10.

Part Number: ADS7138


Tool/software:

Hello,

We are planning to use ADS7138IRTET in one of our design and it gets connected to ZYNQ 7000 FPGA PS which runs on the LINUX Kernel 5.10.

Is the driver available for LINUX kernel 5.10. If yes, can you please provide us the same.

Thanks,

M.J.K.Govind.