This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8684: Small number of convertors seem to be in power down or ext. VREF modes.

Part Number: ADS8684


Tool/software:

The problem is that a minority of ADC8684 circuits do not emit VREF on output or response on MISO.   I am currently exploring if the ADC is in power-down or external VREF modes.  Troublesome, as this can only be diagnosed symptomatically.

Currently investigating if initial power sequencing (or other power characteristic) is source of problem.  Further i am trying to prove or dis-prove that the ADC is interpreting the duration of the *RST/*PD low state relative to Power Supply Levels and ramp time as power down signaling. 

I am comparing those configurations that work vs. those that do not. 

At this time i do not see significant difference between working and non-working ADCs states regarding  *RST/*PD Pin initial positive EDGE (due to 47k to DVDD) and availability and level of either 3.3Vdc (DVDD) or 5Vdc (AVDD) Supplies.