Part Number: DATACONVERTERPRO-SW
Other Parts Discussed in Thread: DAC38J84
Tool/software:
Dear,
Does HSDC Pro Gui has support and work with ZCU102 Evalucation FPGA Board from Xilinx?
Regards
Erivelton Castro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DATACONVERTERPRO-SW
Other Parts Discussed in Thread: DAC38J84
Tool/software:
Dear,
Does HSDC Pro Gui has support and work with ZCU102 Evalucation FPGA Board from Xilinx?
Regards
Erivelton Castro
No, it is designed to work for capture cards released by TI.
Hello,
I received this message saying that you can use the HSDC Pro but need the TSW14J10.
Is it correct this?
Regards
Erivelton Castro
The above thread is to connect dac37j84evm to ZCU102 fpga board instead of TSW14J10 . In that case hsdcpro is not required. You need to write capture code and work with it .
Which is the EVM you want to use ? dac37j84evm does not belong to our group.
Hello,
I'm using this plataform DAC37J84EVM with FPGA ZCU102 EVM board.
This link says that HSDC Pro can be used if TSW14J10 is connected to ZCU102. It is necessary to use TSW14J10 with ZCU102 to work with HSDC Pro. Otherwise, TSW14J10 is not needed if the customer can directly create RTL/VHDL code to send data to the EVM DAC38J84.
Is this information correct?
Follow the link to consult.
Regards,
Erivelton Castro
Yes this is correct . But DAC37J84EVM is not from our group . Can you please post separate e2e mentioning DAC37J84EVM so that appropriate people will respond.