This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102: Input Protection Cross Channel Impact?

Part Number: ADC128S102


Tool/software:

The datasheet for the device says it can handle up to VA+0.3V inputs and even higher if current limited to under 10mA.

I have two inputs to the ADC, that at worst case tolerance stackup could be as high as 5.35V (separate power supply, sequenced to be after VA... But much less precise). These inputs pass through a 100Ohm series resistor before reaching the ADC128S102.

So in theory they could have input current around 3.5mA each, which seems acceptable.

However, I do not want these inputs negatively impacting other channels...

Would this configuration have any negative impact on sampling other channels of the device?