This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS114S06: Is the POR_Flag set on RESET?

Part Number: ADS114S06

Tool/software:

Hi, Staff

I have a question about the POR_Flag of the ADS114S06IPBS.
When a power-on reset occurs, it becomes "1",
but is it also set to "1" by a reset command or by a reset terminal?

regards
cafain

  • Hi Cafain,

    yes, the POR_Flag of ADS114S06 would set to 1b after any type of reset (power-on reset, hardware reset using the RESETn pin, or software reset using the RESET command).
    I should probably have chosen a different name in this case for this status flag.

    Regards,
    Joachim Wuerker