Other Parts Discussed in Thread: ADS1298
Hi,
I read all the previous post related to this subject but there are still some points that are not clear to me.
I would like to use the ADS1298 for measuring and recording EMG signals, beginning with the available ADS1298ECG demonstration board.
From what I understood, EMG signals have the biggest amplitude among the different body signals (Signals) : EMG>ECG>EEG.
In the ADS1298ECG manual, it says that we can directly hook-up ECG signals to ADC inputs without any preamplifier stage for a proper use.
From this app note I understand that only EEG signals will require a preamplification as they are weak and using directly AD converter will bring a lot of noise.
My conclusion is that I would not need any preamplification for EMG signals as their amplitude is higher than ECG, could someone correct me?
Is the PGA stage sufficient for amplifying EMG signals so that the dynamic range could fit with the ADC input?
Could someone advice me on the procedure and stages required to use the ADS1298ECG in the best way possible for EMG measurement?
About the demonstration kit, I understood that I could use it with any microcontroller boards besides the MMB0 as it use a SPI interface.
My question are:
- Could I develop my own application to get the raw data from the ADC channels? Could I use a software like Matlab to plot the data?
- Could I program DSP present on the MMB0 like a microcontroller (C language)? Could I use CCS or IAR?
- If not, could someone advise me on other boards that could be easy to use (microcontroller) with the ADS1298ECG board? Is there a MSP430 development board ready for that? In this case could where could I get the ADS1298ECG board only?
Thanks very much in advance, hope you can provide me these information.
Regards.