Part Number: AFE58JD28
Tool/software:
I use the AFE58JD28 to verify the JESD204B function, test mode transmission BC50H, now the phenomenon is that the first frame of the ILA and the third frame and the fourth frame of the padding data is irregular, and the transmission of the BC50H data is also irregular data, when I skip the ILA can be received by the two channel transmission of the BC50H, will be received by the AFE The problem is the same after disconnecting the SYSREF signal, is it a problem that the AFE is not receiving SYSREF?