Part Number: AFE58JD28
Tool/software:
The SYSREF signal circuit diagram is shown below, I used an oscilloscope to capture the clock as follows
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE58JD28
Tool/software:
The SYSREF signal circuit diagram is shown below, I used an oscilloscope to capture the clock as follows
Hi,
Can you please describe your problem ? Is sysref signal is not detected by device ? Why is p and m signal have different high/low voltage ?
Is it possible to share the sysref circuit ?

Following the AFE58JD28EVM schematic, using an oscilloscope to measure the common mode voltages of _P and _N are different, is there a problem with the provided schematic? Now the phenomenon is that JESD204B enters into the receiving data stage, I set the ADC to test mode and send BC50H, the received data is not BC50H, the phenomenon of providing the SYSREF signal and not providing it is the same, so I suspect that the ADC does not receive the SYSREF
Translated with DeepL.com (free version)
Sysref required from device requries common mode to be 0.7. In the datsheet it is explained how to shift the common mode . This might not be followed on EVM . In that case you see the difference is sysrefp and sysrefm min and max value.
No, sysref should not cause this . You can use adc test mode such as ramp/ toggle pattern/ constant pattern to see at the output
Also, I would like to ask what is the data format of the first frame of the ILA transmission phase of the AFE58JD28 JESD? I know the second frame transmits link configuration data, is the data in the first frame arbitrary?
Because I saw in one of TI's explanatory documents that the first frame is the sum number