Hi folks:
I am ramping up some work involving the ADS1298 ECG analog front-end device.
When I read the ID register on the ADS1298, I get 52h. From the description of the ID register (address: 00h) on page 46 of the ADS129x datasheet, I expect ID=92h.
However, in section 5.9 "Register Map" of the ADS1298ECG-FE Performance Demonstration Kit User's Guide (SBAU171A), the value for the ID register is listed as 0x52, which is the same value I get.
I inherited a custom prototype setup using the following:
a) TMS320C5515 EVM assembly 512700 rev B
b) Actel AGLN250 nano FPGA starter kit board
c) ADS1298ECG-FE Performance Demonstration Kit rev A with ADS1298ZXG 9AZEZ89GJ
Is ID=52h correct for ADS1298ZXG 9AZEZ89GJ ?
Do I have a problem that I should resolve?
Thanks in advance for any guidance!
PJ