Tool/software:
Hi, TI expert
I have a question from a customer about ADS1292IPBS.
The customer is developing a Holter ECG using the internal clock (512kHz) of ADS1292.
The internal clock accuracy is expressed as below on the datasheet (0.5%), but the error of the actual measured data is larger than the customer's specification (0.03%), which is causing a problem.

Q1) Can the error range be reduced by using an external clock?
Q2) Is there a way to reduce the error range when using an internal clock? (The relevant AFE circuit diagram is attached below.)
Q3) Can you recommend a crystal that can reduce the error of the external clock?

Please check. Thanks