Part Number: ADS52J65
Tool/software:
Dear TI team
I have some question about the Analog input in ADS52J65
In the datasheet file
Page 29
“For a full-scale differential input, each input pin INP, INM must swing
symmetrically between VCM + 0.5 V and VCM – 0.5 V, resulting in a 2-Vpp differential input swing.”
But (VCM + 0.5 V) – (VCM - 0.5 V) = 1V not 2-Vpp
Same recommendation in page 7
Page 6
Absolute Maximum Ratings
Voltage applied to
analog input pins AINMx, AINPx –0.3 minimum ( 2.2, AVDD_1P8V + 0.3 ) V
If VCM = 0.9V the maximum AINP , AINM as in page 29 will be 1.4V
Our input signal is from power detector Vhigh = 1.27V Vlow = 0.47V swing of 0.8V