Part Number: TLC2578
Other Parts Discussed in Thread: TLC2574, , ADC128S102
Tool/software:
Hello,
I have my ADC and Controller both on different PCBs.
ADC is on High Voltage Section(36KV) so to isolate I wanted to use Fiber Optic links to communicate with ADC.
Limitation of Fiber Optic links is, they are unipolar in nature. Protocols like I2C need bidirectional communication so it seems SPI is the only option.
I have another limitation I can't use 4 Fiber Optic links for CLK, CS, SDO and SDI in SPI comm. I have a limitation of 3.
In TLC2574 / 8 it is mentioned user can tie CS to permanently low, that leaves my Fiber Optic connector requirement to 3 (Two transmitters for SCLK and SDI and one receiver for SDO at Controller end).
Is it the correct way?
Any other suggestions or devices? My requirement is minimum 200ksps, 12bit, 4 channel or 8 channel.
Thanks,