This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ABACO-3P-FMC160: Dual-Polarity support

Part Number: ABACO-3P-FMC160

Tool/software:

I would like to ask about whether the ABACO-3P-FMC160 can support dual polarity or not. In other words, can It accept negative AC values?

Also concerning the Input Range, It is mentioned that it supports 0.8V p.p. Does that mean that the signal can swing from 0 to 0.8V or from -0.4 to 0.4?

Thank you very much.