Part Number: ADS131M08
Tool/software:
hello TI experts,


Question 1: if configuring bit 6 of CLOCK Register to 1 will physically disconnect the 1.2V internal reference within the ADS131M08 chip (through a switch like mechanism)?

Question 2: According to the data manual, when using an external reference of 1.25V, the actual ADC full-scale range is 1.2V/gain PGA; But the reference voltage of 1.3V is 1.248V/gain PGA. May I ask how 1.25V corresponds to 1.2V/gain and 1.3V corresponds to 1.248V/gain, which are not described in the manual.