This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: About the IBW of 20 GSPS application

Part Number: ADC12DJ5200RF


Tool/software:

Hi expert,

If 2 interleaving ADC be used, then the Fs is about 20 GSPS, is the IBW approximately Fs/2 = 10 GSPS ?

Thanks.

  • Hi Ryan,

    The effective sample rate would be 20GSPS and the nyquist rate would then be 10GSPS. But you won’t be able to sample signals outside the bandwidth of the ADC linearly. Refer to the datasheet bandwidth plot (Figure 5-1) to see the bandwidth of the ADC begin to drop at 8GHz. In doing this, you will need to implement some interleaving correction algorithm. Our advice is to ensure that the analog board design is as perfectly aligned as possible which should help make the correction easier.

    Thanks, Chase