Part Number: DAC8820EVM
Other Parts Discussed in Thread: REF102, INA105, DAC8820
Tool/software:
I am not able to get this board working as expected. I suspect the board is malfunctioning
Datasheet /user guide here:
- +VA =15V,
- -VA= -15V
- also supplied are +5V, and +3.3V.
- I am using the onboard reference
- I am not using the reference inverter (jump W1 moved to +Ref position)
- The Test point RefTest says ~+8.6V (not +10V)
- Something on the board near the reference is heating up the board
- i do not think it is ther reference itself as it doesn't feel as hot as the board near it if i touch it (after turning off)
- The output reads ~ -8.6 V (Which would be consistent with 0-code DAC if the reference was ~8.6 V as measured)
I think maybe capacitor C1 is failing or broken. The user guide says capacitor C1 (C1608X5R1A105K) is only rated to 10V. However, this seems crazy since you obviously REF102 requires Vin between 11V and15V.