Other Parts Discussed in Thread: AFE5807, AFE5807EVM
ADS807E is used in our design, to convert analog input to digital output, expected to work with 50 MHz clock input.
We have referred the design used in DEM-ADS807E Evaluation kit (http://www.ti.com/lit/ug/sbau007/sbau007.pdf)
Problem faced: When an input signal (reference voltage) is given to the input, in the expected digital output most of the bits are oscillating, only the bit which is high is constantly high. If only few LSB was oscillating then it could be the high accuracy reading of the ADC but no matter what bit it is, if it not high than it keeps oscillating from high to low vice versa.