This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE2256EVM: Error: Oops! Header file not found

Part Number: AFE2256EVM
Other Parts Discussed in Thread: AFE2256

Tool/software:

Hi Experts,

I have got the afe2256evm. but when I tested it (all one's pattern), it got the error: oops header data not found. I just installed one afe2256, is that right? 

I install your software on win10. I correctly installed the USB, firmware, I want to get the image. But I only got the error: oops header data not found.

I just installed one afe2256 on the board. even if I use the all-one test pattern, it's the same. Though it notified has error, but I tested the SPI configuration is ok!, so I think it does not matter. 



Please advise.

Regards,

Josel

  • Hi Josel,

    The AFE2256EVM's data capture can operate correctly only when both the AFE2256 COFs are connected to the EVM. Can you connect the other adapter card as well, restart the GUI and retry the data capture?

    Please let me know if you still see the issue.

    Thanks & Regards,

    Aditya