Part Number: ADS52J90
Other Parts Discussed in Thread: THS4551, THS4509
Tool/software:
Hello,
I have a couple of quick questions regarding the ADC input stage in the ADS52J90:
1) I'm trying to simulate the ADC input stage as per the schematic in the datasheet (Figure 91, page 72). Could you please be so kind and provide me with the acquisition time and the conversion time?
The ADC will be running at 30MSPS.
2) I know the EVM recommends a THS4509RGTR for the input, but at roughly 38mA per channel, 64 channels would take a lot of power. In our application, the input signal frequency will not exceed 2.5MHz, and we are planning on running the ADC at 30MSPS, 14 bits, 64 channels. So the question is: would a THS4551 be fast enough for our application? Or, perhaps you could recommend another opamp with lower power consumption than the THS4509? Anything with an Iq lower than 10mA would be great.
Thank you very much!
Vlad Ardelean