Tool/software:
Hello,
I went through the datasheet over and over and am still confused about the analog input range.
I want to use hardware programming.
I understand in Hardware mode the ADC is forced into High Reference Range.
Somewhere else I read that in High Reference range, the ADC is forced to +/-VREF (so +/-2VREF is not possible).
So in Hardware Programming mode, the ADC is ALWAYS in High Reference Range and +/-VREF range.
I found in fig-2-1 of the EVM Manual the lower right curve, single ended 5V pp at 2.5V offset. But not if that is for +/-REF or +/-2VREF.
I want a span of -2.048 V to +2.048 V (4.096 V pp) around +2.5V.
Do I need a VREF+ of 2.048V or 4.096 V??
(VREF- is connected to AVSS)