This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1118: The ADC promoted

Part Number: ADS1118

Tool/software:

Hi,

We need to choose the ADC for the single sampling, and the spec. request as below:

1. The input voltage range -100mV ~ 100mV;

2. The temperature accuracy +/- 0.05%;

3. The 2 channels total response time less than 10mS( 2*(Sampling time + conversion time + SPI communication time) < 10mS);

We search the ADS1118 is well for our request but the voltage range is ±0.256 V min, it maybe not suitable for the input voltage -100mV ~ 100mV,

can you help to promote the other ADC to us for this request, thanks.