Part Number: ADC3910D065
Other Parts Discussed in Thread: ADC3910D125EVM, TSW1418EVM,
Tool/software:
Trying to load the FPGA for the capture card and get these errors:
"Enable end of startup check" Box checked:
ERROR: [Labtools 27-3165] End of startup status: LOW
ERROR: [Common 17-39] 'program_hw_devices' failed due to earlier errors.
ERROR: [Labtoolstcl 44-513] HW Target shutdown. Closing target: localhost:3121/xilinx_tcf/Digilent/210249BAC1C1
or
"Enable end of startup check" Box unchecked:
ERROR: [Labtools 27-2312] Device xc7a100t_0 is no longer available.
Check cable connectivity and that the target board is powered up then
use the disconnect_hw_server and connect_hw_server to re-initialize the hardware target.
Use open_hw_target to re-register the hardware device.
ERROR: [Labtoolstcl 44-513] HW Target shutdown. Closing target: localhost:3121/xilinx_tcf/Digilent/210249BAC1C1
Then a power cycle of the card is required but still has this error.
Using Vivado 2022.2
Thanks,
Jon